Hi team,
I have questions related to the supported application, specifically Aerospace.
TMS320F28377D-EP datasheet clearly states “Supports Defense, Aerospace, and Medical Applications”. Also TMS320F28377D-EP’s temp range is extended to -55 to 125 ℃.
On the other hand, TMS320F28377D datasheet does not say it supports Aerospace, and it has lower temp limit as -40.
My questions are:
Does TMS320F28377D support Aerospace application?
If -40℃ is enough for the system, can I use TMS320F28377D for Aerospace application?
What is the difference between device supports Aerospace and device does not support Aerospace?
Best regards,
Kurumi Hasegawa