This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC1004EVM: How to solve "No USB FET was found"?

Part Number: FDC1004EVM
Other Parts Discussed in Thread: MSP430F5528, FDC2214EVM, MSP-FET, ENERGIA, MSP430F5529

I have FDC1004EVM, and I am trying to do the same thing as the old thread, The FDC 1004EVM has MSP430F5528 controller, however, the Eenergia IDE has MSPF5529 selection. I got the same error messages below. The Board is connected as it has LED on and also show in the right-bottom corner  .

The same thing occurs when I tried FDC2214EVM. 

Can someone help me with the issue?

=================

Sketch uses 6932 bytes (14%) of program storage space. Maximum is 48128 bytes.
Global variables use 304 bytes (3%) of dynamic memory, leaving 7888 bytes for local variables. Maximum is 8192 bytes.
DSLite version 9.3.0.1863
Configuring Debugger (may take a few minutes on first launch)...
Initializing Register Database...
Initializing: MSP430
error: MSP430: Error initializing emulator: No USB FET was found
Failed: MSP430: Error initializing emulator: No USB FET was found

the selected serial port
does not exist or your board is not connected

**Attention** This is a public forum