Part Number: MSP430F5529
Other Parts Discussed in Thread: MSP-EXP430F5529LP, ENERGIA, UNIFLASH
Energia: 1.8.7E21 (Windows 10), Board: "MSP-EXP430F5529LP"
Sketch uses 1206 bytes (2%) of program storage space. Maximum is 48128 bytes.
Global variables use 18 bytes (0%) of dynamic memory, leaving 8174 bytes for local variables. Maximum is 8192 bytes.
DSLite version 8.2.0.1400
Configuring Debugger (may take a few minutes on first launch)...
Initializing Register Database...
Initializing: MSP430
error: MSP430: Error initializing emulator: No USB FET was found
Failed: MSP430: Error initializing emulator: No USB FET was found
the selected serial port
does not exist or your board is not connected
This report would have more information with
"Show verbose output during compilation"
option enabled in File -> Preferences.
How do I fix this?