Other Parts Discussed in Thread: MSP430FR5994
Hi,
I have bought MSP430FR5994 and BOOSTXL-AUDIO. So I started off by checking the schematics of BOOSTXL-AUDIO. I found that there is some misconnections in that.
1)Speaker Terminal is shorted and connected to the same pin of the IC.
2)Both the input and output pins from microphone amplifier is connected to one terminal of microphone.
My questions are,
1)How should I start with that, like programming?
2)What and How can I execute any example program and test BOOSTXL-AUDIO, if it is working or not? (I tested MSP430FR5994 by simply running a LED BLINK code)
3)Can I program my device even if there is misconnections?(I doubt IF it will work)
4)What can I do to correct those misconnections? Can I return it? If so how?
Thanks and Regards,
Nivethitha D