This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Could you tell me about the effective number of bits in MSP430I2020.
A resolution that can divide 10000 of Min 1g and Max 10000g is required.
Thanks,
Koki
Hi,
The calculation was based on your feedback (ENOB = ((SINAD -1.76)) / (6.02 dB)).
Then, when 89db, ENOB is 14.5bit.
and when 77db, ENOB is 12.5bit.
i2020 ENOB is arround 16-17bit depends on the different gain setting.
How did you calculate the above values?
Thanks,
Koki
Hi,Koki,
You are correct for i2020. You need check if the resolution is enough or not.
**Attention** This is a public forum