This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My target is MSP430F5529 & IDE is IAR EWB, I am developing a custom BSL which will not have any communication, it just need to check for new firmware on external EEPROM & load it to flash. I changed the file "BSL430_Low_Level_Init.s43" available in example MSP430F552x 00.05.84.34 to disable USB functionality.
I could able to build completely. Now when I try to debug without downloading, I am getting the error "Illegal op-code found on address 0x0". I have unchecked the run to main option in Debugger selection. Please suggest what could be the problem.
Thanks
Gireesh
Hi,
This error message can be ignored, and happens when you download BSL startup code to the simulator. Set the PC to the starting point of your low level init code, and you can debug as you'd like.
**Attention** This is a public forum