I have one MSP430F5529LP. I want to update firmware by UART BSL.
I try those method, but still fail.
My MSP430F5529 hardware connect to PC path on below:
MSP430F5xxx <--> FT232 <------> USB <-------->PC
RX --- TX
TX --- RX
TST/SBWTCK --- RTS
GND --- GND
RST/SBWTDIO --- DTR
1. When I use python-msp430-tools. I try any command, but always no response. such as python -m msp430.bsl5.uart -p COM17 -e.
I also try python -m msp430.bsl5.uart -p COM17 --invert-test. But my test pin no invert.
2. I also use BSL_Scripter.exe, but still fail. It always response no ack.
3. I try to use software entry BSL then using BSL_Scripter.exe or python-msp430-tools still fail.
In my main.c. I write
__disable_interrupt(); // disable interrupts
((void ( * )())0x1000)(); // jump to BSL
Can't anyone tell me how should I do?
Thanks.