This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2013: About the single chip analog input of MSP430F2013 chip

Part Number: MSP430F2013


Hi team,

I got a question about SD16_A in MSP430F2013 from customer.

QS1:
If I use a single input of analog-to-digital converter. If I use the on-chip reference voltage generation (1.2 V), the signal input in A4+, and A4- connect to GND, weather the maximum full-scale input range for a gain of 1 is ±0.6V ? If I connect a 0.4V to A4-, what is the maximum full-scale input range for a gain of 1?

QS2:
In the schematic, it use P2.6 as a analog output, how to realize P2.6 as analog output? What is it range?


QS3:
I notice it use P1.0 P1.4 P1.5 connect to a anode of a thermal pile with different resistor, why it do this?

Thank you very much for your help.

Best regards,

**Attention** This is a public forum