This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-GANG: "ERROR 308: Communication Port baud rate change" & selftest fail

Part Number: MSP-GANG

My customer has reported the same phenomenon that has been posted on E2E before.
"MSP-GANG: MSP-GANG programmer can't pass selftest".
Can you please let us know what the final solution will be?

The site is Locked and I can't see the content.

  • Hi Yasutoshi,

    You cancheck the wire between MSP-GANG and MCU, if this wire too long will have some error.

    And self test should will report some comments, you can refer this comments to find the root cause.

    UG(Page54): https://www.ti.com/lit/ug/slau358q/slau358q.pdf

    Thanks!

    Best Regards

    Johnson

  • Hi Johnson,

    Thanks for the quick reply.
    This time, the customer has already performed the Self Test by connecting the MSP-GANG to the USB port of the PC,
    but it seems that the Self Test cannot be performed in the first place as shown below.
    Is this purely a problem with the USB port of the PC?

     

  • Hi Yasutoshi,

    I find this MSP-GANG don't have the basic information, like Hardware Num, Slilcon number, it seems very stranger.

    Where did the customer get this MSP-GANG?

    Thanks!

    Best Regards

    Johnson

  • Hi Johnson,


    The customer has two MSP-GANGs. One of them is HW Revision 1.04, and the other one is HW Revision 1.05, which they purchased this time.They purchased both of them from us.

    According to the customer's report, the customer's one PC (BBC-1010-H7D-W7) does not show any information on the Self Test for both MSP-GANGs, as shown in the previous result.

    However, when the customer ran the Self Test on another PC (SIMATIC IPC647C), the result was working fine as below.

    Therefore, I feel that the connection between the USB port of the PC (BBC-1010-H7D-W7) used by the customer and the MSP-GANG may be causing some problems, but have there been any reports of similar phenomena?

  • Hi Yasutoshi,

    I agree with you, maybe the issue is cause by MSP-GANG driver in PC (BBC-1010-H7D-W7), you can try to uninstall this driver and install again.

    Thanks!

    Best Regards

    Johnson

  • Hi Johnson,

    Thanks for you feedbacks.

    === MSP-GANG Self test results ( Monday, September 20, 2021,  13:30:30 ) ===
    
    Adapter SN ------:  20070444 
    Hardware --------:  G430:  01.05
    Access key ------:  MSP-GANG Programmer 
    Silicon Number --:  588C 886E 1700 1C00
    API Firmware ----:  MSP-Gang   A430:  01.02.10.00
    BOOT Firmware ---:  G430BOOT   B430:  01.00.02.00
    GUI Software ----:  MSP-Gang-GUI   G430:  01.02.10.00
    DLL Software ----:  MSP-Gang-DLL   D430:  01.02.10.00
    
    ================ Test results =============
    
    
    No.       name                   parameter       limits               result         status
    
    
      1: Data Bus   (ALL LOW)          0x0000   (0x0000  - 0x0000)  Result:  0x00     ... >>  OK   <<
      2: Data Bus   (ALL HIGH)         0x00FF   (0xFFFF  - 0xFFFF)  Result:  0xFFFF   ... >>  OK   <<
      3: Data Bus   (D-0 HI )          0x0001   (0x0101  - 0x0101)  Result:  0x0101   ... >>  OK   <<
      4: Data Bus   (D-1 HI )          0x0002   (0x0202  - 0x0202)  Result:  0x0202   ... >>  OK   <<
      5: Data Bus   (D-2 HI )          0x0004   (0x0404  - 0x0404)  Result:  0x0404   ... >>  OK   <<
      6: Data Bus   (D-3 HI )          0x0008   (0x0808  - 0x0808)  Result:  0x0808   ... >>  OK   <<
      7: Data Bus   (D-4 HI )          0x0010   (0x1010  - 0x1010)  Result:  0x1010   ... >>  OK   <<
      8: Data Bus   (D-5 HI )          0x0020   (0x2020  - 0x2020)  Result:  0x2020   ... >>  OK   <<
      9: Data Bus   (D-6 HI )          0x0040   (0x4040  - 0x4040)  Result:  0x4040   ... >>  OK   <<
     10: Data Bus   (D-7 HI )          0x0080   (0x8080  - 0x8080)  Result:  0x8080   ... >>  OK   <<
    
     11: Data-2 Bus  (ALL LOW)         0x0000   (0x0000  - 0x0000)  Result:  0x00     ... >>  OK   <<
     12: Data-2 Bus  (ALL HIGH)        0x00FF   (0xFFFF  - 0xFFFF)  Result:  0xFFFF   ... >>  OK   <<
     13: Data-2 Bus  (D2-0 HI )        0x0001   (0x0101  - 0x0101)  Result:  0x0101   ... >>  OK   <<
     14: Data-2 Bus  (D2-1 HI )        0x0002   (0x0202  - 0x0202)  Result:  0x0202   ... >>  OK   <<
     15: Data-2 Bus  (D2-2 HI )        0x0004   (0x0404  - 0x0404)  Result:  0x0404   ... >>  OK   <<
     16: Data-2 Bus  (D2-3 HI )        0x0008   (0x0808  - 0x0808)  Result:  0x0808   ... >>  OK   <<
     17: Data-2 Bus  (D2-4 HI )        0x0010   (0x1010  - 0x1010)  Result:  0x1010   ... >>  OK   <<
     18: Data-2 Bus  (D2-5 HI )        0x0020   (0x2020  - 0x2020)  Result:  0x2020   ... >>  OK   <<
     19: Data-2 Bus  (D2-6 HI )        0x0040   (0x4040  - 0x4040)  Result:  0x4040   ... >>  OK   <<
     20: Data-2 Bus  (D2-7 HI )        0x0080   (0x8080  - 0x8080)  Result:  0x8080   ... >>  OK   <<
    
     21: Vcc Target-1 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.02 V   ... >>  OK   <<
     22: Vcc Target-2 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
     23: Vcc Target-3 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
     24: Vcc Target-4 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
     25: Vcc Target-5 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
     26: Vcc Target-6 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
     27: Vcc Target-7 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
     28: Vcc Target-8 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
    
     29: Translators VT (OFF)           0.00 V  (  0.00 to   0.50)  Result:  0.01 V   ... >>  OK   <<
     30: Translators VT (ON 1.8V)       1.80 V  (  1.60 to   2.00)  Result:  1.77 V   ... >>  OK   <<
     31: Translators VT (ON 2.7V)       2.70 V  (  2.50 to   2.90)  Result:  2.64 V   ... >>  OK   <<
     32: Translators VT (ON 3.6V)       3.60 V  (  3.40 to   3.80)  Result:  3.51 V   ... >>  OK   <<
    
     33: Vpp Voltage-in                10.00 V  (  8.00 to  12.00)  Result: 10.23 V   ... >>  OK   <<
     34: Vpp Voltage                    7.00 V  (  6.50 to   7.30)  Result:  6.89 V   ... >>  OK   <<
     35: Internal Vcc-3.3V              3.30 V  (  3.20 to   3.40)  Result:  3.31 V   ... >>  OK   <<
    
     36: Vcc Target-1 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.80 V   ... >>  OK   <<
     37: Vcc Target-2 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.82 V   ... >>  OK   <<
     38: Vcc Target-3 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.79 V   ... >>  OK   <<
     39: Vcc Target-4 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.80 V   ... >>  OK   <<
     40: Vcc Target-5 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.80 V   ... >>  OK   <<
     41: Vcc Target-6 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.81 V   ... >>  OK   <<
     42: Vcc Target-7 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.80 V   ... >>  OK   <<
     43: Vcc Target-8 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.79 V   ... >>  OK   <<
     44: Vcc Target-1 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.68 V   ... >>  OK   <<
     45: Vcc Target-2 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.70 V   ... >>  OK   <<
     46: Vcc Target-3 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.67 V   ... >>  OK   <<
     47: Vcc Target-4 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.69 V   ... >>  OK   <<
     48: Vcc Target-5 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.68 V   ... >>  OK   <<
     49: Vcc Target-6 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.69 V   ... >>  OK   <<
     50: Vcc Target-7 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.67 V   ... >>  OK   <<
     51: Vcc Target-8 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.67 V   ... >>  OK   <<
     52: Vcc Target-1 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.55 V   ... >>  OK   <<
     53: Vcc Target-2 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.59 V   ... >>  OK   <<
     54: Vcc Target-3 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.56 V   ... >>  OK   <<
     55: Vcc Target-4 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.57 V   ... >>  OK   <<
     56: Vcc Target-5 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.57 V   ... >>  OK   <<
     57: Vcc Target-6 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.58 V   ... >>  OK   <<
     58: Vcc Target-7 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.56 V   ... >>  OK   <<
     59: Vcc Target-8 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.55 V   ... >>  OK   <<
    
     60: Vcc discharge (100ms)Target-1  3.60 V  (  1.00 to   2.70)  Result:  1.19 V   ... >>  OK   <<
     61: Vcc discharge (100ms)Target-2  3.60 V  (  1.00 to   2.70)  Result:  1.16 V   ... >>  OK   <<
     62: Vcc discharge (100ms)Target-3  3.60 V  (  1.00 to   2.70)  Result:  1.19 V   ... >>  OK   <<
     63: Vcc discharge (100ms)Target-4  3.60 V  (  1.00 to   2.70)  Result:  1.21 V   ... >>  OK   <<
     64: Vcc discharge (100ms)Target-5  3.60 V  (  1.00 to   2.70)  Result:  1.17 V   ... >>  OK   <<
     65: Vcc discharge (100ms)Target-6  3.60 V  (  1.00 to   2.70)  Result:  1.20 V   ... >>  OK   <<
     66: Vcc discharge (100ms)Target-7  3.60 V  (  1.00 to   2.70)  Result:  1.19 V   ... >>  OK   <<
     67: Vcc discharge (100ms)Target-8  3.60 V  (  1.00 to   2.70)  Result:  1.19 V   ... >>  OK   <<
    
     68: Vcc Target-1 ( #1 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.26 V   ... >>  OK   <<
     69: Vcc Target-2 ( #1 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     70: Vcc Target-3 ( #1 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     71: Vcc Target-4 ( #1 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     72: Vcc Target-5 ( #1 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     73: Vcc Target-6 ( #1 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     74: Vcc Target-7 ( #1 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     75: Vcc Target-8 ( #1 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     76: Vcc Target-1 ( #2 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.17 V   ... >>  OK   <<
     77: Vcc Target-2 ( #2 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.29 V   ... >>  OK   <<
     78: Vcc Target-3 ( #2 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     79: Vcc Target-4 ( #2 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     80: Vcc Target-5 ( #2 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     81: Vcc Target-6 ( #2 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     82: Vcc Target-7 ( #2 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     83: Vcc Target-8 ( #2 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     84: Vcc Target-1 ( #3 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     85: Vcc Target-2 ( #3 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     86: Vcc Target-3 ( #3 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.26 V   ... >>  OK   <<
     87: Vcc Target-4 ( #3 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     88: Vcc Target-5 ( #3 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     89: Vcc Target-6 ( #3 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     90: Vcc Target-7 ( #3 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     91: Vcc Target-8 ( #3 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     92: Vcc Target-1 ( #4 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     93: Vcc Target-2 ( #4 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     94: Vcc Target-3 ( #4 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     95: Vcc Target-4 ( #4 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.28 V   ... >>  OK   <<
     96: Vcc Target-5 ( #4 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     97: Vcc Target-6 ( #4 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     98: Vcc Target-7 ( #4 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     99: Vcc Target-8 ( #4 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    100: Vcc Target-1 ( #5 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    101: Vcc Target-2 ( #5 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    102: Vcc Target-3 ( #5 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    103: Vcc Target-4 ( #5 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    104: Vcc Target-5 ( #5 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.27 V   ... >>  OK   <<
    105: Vcc Target-6 ( #5 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    106: Vcc Target-7 ( #5 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    107: Vcc Target-8 ( #5 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    108: Vcc Target-1 ( #6 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    109: Vcc Target-2 ( #6 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    110: Vcc Target-3 ( #6 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    111: Vcc Target-4 ( #6 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    112: Vcc Target-5 ( #6 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    113: Vcc Target-6 ( #6 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.28 V   ... >>  OK   <<
    114: Vcc Target-7 ( #6 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    115: Vcc Target-8 ( #6 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    116: Vcc Target-1 ( #7 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    117: Vcc Target-2 ( #7 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    118: Vcc Target-3 ( #7 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    119: Vcc Target-4 ( #7 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    120: Vcc Target-5 ( #7 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    121: Vcc Target-6 ( #7 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    122: Vcc Target-7 ( #7 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.26 V   ... >>  OK   <<
    123: Vcc Target-8 ( #7 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    124: Vcc Target-1 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    125: Vcc Target-2 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    126: Vcc Target-3 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    127: Vcc Target-4 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    128: Vcc Target-5 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    129: Vcc Target-6 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    130: Vcc Target-7 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    131: Vcc Target-8 ( #8 ON )         3.30 V  (  3.10 to   3.50)  Result:  3.25 V   ... >>  OK   <<
    
    132: SD Power OFF                  0x0000   (0x0000  - 0x0000)  Result:  0x00     ... >>  OK   <<
    133: SD Power ON                   0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    134: SD Discharge -  delay 2ms     0x0010   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    135: SD Discharge -  delay 50ms    0x0010   (0x0000  - 0x0000)  Result:  0x00     ... >>  OK   <<
    
    136: BSL RX bus (#1 HIGH)          0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    137: BSL RX bus (#2 HIGH)          0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
    138: BSL RX bus (#3 HIGH)          0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
    139: BSL RX bus (#4 HIGH)          0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
    140: BSL RX bus (#5 HIGH)          0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
    141: BSL RX bus (#6 HIGH)          0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
    142: BSL RX bus (#7 HIGH)          0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
    143: BSL RX bus (#8 HIGH)          0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<
    
    144: BSL TX bus (#1 HIGH)          0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    145: BSL TX bus (#2 HIGH)          0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
    146: BSL TX bus (#3 HIGH)          0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
    147: BSL TX bus (#4 HIGH)          0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
    148: BSL TX bus (#5 HIGH)          0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
    149: BSL TX bus (#6 HIGH)          0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
    150: BSL TX bus (#7 HIGH)          0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
    151: BSL TX bus (#8 HIGH)          0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<
    
    152: TDI bus  (#1 HIGH)            0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    153: TDI bus  (#2 HIGH)            0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
    154: TDI bus  (#3 HIGH)            0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
    155: TDI bus  (#4 HIGH)            0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
    156: TDI bus  (#5 HIGH)            0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
    157: TDI bus  (#6 HIGH)            0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
    158: TDI bus  (#7 HIGH)            0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
    159: TDI bus  (#8 HIGH)            0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<
    
    160: TDOI Tx-bus (#1 HIGH)         0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    161: TDOI Tx-bus (#2 HIGH)         0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
    162: TDOI Tx-bus (#3 HIGH)         0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
    163: TDOI Tx-bus (#4 HIGH)         0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
    164: TDOI Tx-bus (#5 HIGH)         0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
    165: TDOI Tx-bus (#6 HIGH)         0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
    166: TDOI Tx-bus (#7 HIGH)         0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
    167: TDOI Tx-bus (#8 HIGH)         0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<
    
    168: TDOI Tx-Rx (#1 HIGH)          0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    169: TDOI Tx-Rx (#2 HIGH)          0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
    170: TDOI Tx-Rx (#3 HIGH)          0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
    171: TDOI Tx-Rx (#4 HIGH)          0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
    172: TDOI Tx-Rx (#5 HIGH)          0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
    173: TDOI Tx-Rx (#6 HIGH)          0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
    174: TDOI Tx-Rx (#7 HIGH)          0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
    175: TDOI Tx-Rx (#8 HIGH)          0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<
    
    176: TDOI Rx-bus (#1 HIGH)         0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    177: TDOI Rx-bus (#2 HIGH)         0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
    178: TDOI Rx-bus (#3 HIGH)         0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
    179: TDOI Rx-bus (#4 HIGH)         0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
    180: TDOI Rx-bus (#5 HIGH)         0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
    181: TDOI Rx-bus (#6 HIGH)         0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
    182: TDOI Rx-bus (#7 HIGH)         0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
    183: TDOI Rx-bus (#84 HIGH)        0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<
    
    184: TMS bus (All HIGH)            0x00FF   (0x00FF  - 0x00FF)  Result:  0xFF     ... >>  OK   <<
    185: TMS bus (All LOW)             0x0000   (0x0000  - 0x0000)  Result:  0x00     ... >>  OK   <<
    
    186: TMS bus (#1 HIGH)             0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    187: TMS bus (#2 HIGH)             0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
    188: TMS bus (#3 HIGH)             0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
    189: TMS bus (#4 HIGH)             0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
    190: TMS bus (#5 HIGH)             0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
    191: TMS bus (#6 HIGH)             0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
    192: TMS bus (#7 HIGH)             0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
    193: TMS bus (#8 HIGH)             0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<
    
    194: RST bus (All HIGH)            0x00FF   (0x00FF  - 0x00FF)  Result:  0xFF     ... >>  OK   <<
    195: RST bus (All LOW)             0x0000   (0x0000  - 0x0000)  Result:  0x00     ... >>  OK   <<
    
    196: RST bus (#1 HIGH)             0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    197: RST bus (#2 HIGH)             0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
    198: RST bus (#3 HIGH)             0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
    199: RST bus (#4 HIGH)             0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
    200: RST bus (#5 HIGH)             0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
    201: RST bus (#6 HIGH)             0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
    202: RST bus (#7 HIGH)             0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
    203: RST bus (#8 HIGH)             0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<
    
    204: Keys buffer (All pull-up)     0x001F   (0x001F  - 0x001F)  Result:  0x1F     ... >>  OK   <<
    
    205: Access to LCD RAM (0xAA)      0x00AA   (0x00AA  - 0x00AA)  Result:  0xAA     ... >>  OK   <<
    206: Access to LCD RAM (0x99)      0x0099   (0x0099  - 0x0099)  Result:  0x99     ... >>  OK   <<
    
    207: Image Flash Access (get ID)   0x0002   (0x0001  - 0x0003)  Result:  0x00     ... >> ERROR <<
    
    208: TDI Fuse keys (#1 ON)         0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    209: TDI Fuse keys (#2 ON)         0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
    210: TDI Fuse keys (#3 ON)         0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
    211: TDI Fuse keys (#4 ON)         0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
    212: TDI Fuse keys (#5 ON)         0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
    213: TDI Fuse keys (#6 ON)         0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
    214: TDI Fuse keys (#7 ON)         0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
    215: TDI Fuse keys (#8 ON)         0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<
    
    216: TEST Fuse keys (All OFF )      0.00    (  0.00 to   0.30)  Result:  0.00     ... >>  OK   <<
    217: TEST Fuse keys (#1 ON)         1.00    (  0.80 to   3.00)  Result:  1.26     ... >>  OK   <<
    218: TEST Fuse keys (#2 ON)         2.00    (  0.80 to   3.00)  Result:  1.30     ... >>  OK   <<
    219: TEST Fuse keys (#3 ON)         3.00    (  0.80 to   3.00)  Result:  1.30     ... >>  OK   <<
    220: TEST Fuse keys (#4 ON)         4.00    (  0.80 to   3.00)  Result:  1.29     ... >>  OK   <<
    221: TEST Fuse keys (#5 ON)         5.00    (  0.80 to   3.00)  Result:  1.28     ... >>  OK   <<
    222: TEST Fuse keys (#6 ON)         6.00    (  0.80 to   3.00)  Result:  1.27     ... >>  OK   <<
    223: TEST Fuse keys (#7 ON)         7.00    (  0.80 to   3.00)  Result:  1.25     ... >>  OK   <<
    224: TEST Fuse keys (#8 ON)         8.00    (  0.80 to   3.00)  Result:  1.24     ... >>  OK   <<
    
    ============== Finished =================================
    *  Test failed!!  1 error(s).
    =========================================================
    

    Let me ask one more question.

    Customer try to use the RS232C connection instead of the USB cable connection, but It seem to be getting one error, what is the cause of the following error?  I can't find any details in the documentation, so could you please advise?

     

  • Hi Yasutoshi,

    This error look like can access image, do you store some image in MSP-GANG?

    Thanks!

    Best Regards

    Johnson

  • Johnson,

    Sorry, what do you mean "can access image"?

  • sorry, is cannot. do you store some image in MSP-GANG?

    I can do some test in my side via RS323 interface

  • Do you men we need to save the image in advance when we run the Self Test?

    I will check with the customer if this is the case.

  • Hi Johnson,

    Sorry for multiple update. But, I will share you with the latest information again.
    I asked the customer to use the latest version (MSP-GANG-SOFTWARE_1.03.04.00) and run a Self Test to check the operation status.
    The following two cases were performed on the PC (BBC-1010-H7D-W7) where the problem occurred.


    1) Connected MSP-GANG to USB and performed Self Test

    === MSP-GANG Self test results ( Friday, September 24, 2021,  15:32:06 ) ===
    
    Adapter SN ------:   
    Hardware --------:  :  00.00
    Access key ------:   
    Silicon Number --:  0000 0000 0000 0000
    API Firmware ----:     0000:  00.00.00.00
    BOOT Firmware ---:     0000:  00.00.00.00
    GUI Software ----:  MSP-Gang-GUI   G430:  01.03.04.00
    DLL Software ----:  MSP-Gang-DLL   D430:  01.03.04.00
    
    ================ Test results =============
    
    
    No.       name                   parameter       limits               result         status
    
    
      1: Data Bus   (ALL LOW)          0x0000   (0x0000  - 0x0000)  Result:  0x00     ... >>  OK   <<
    
    ===== Communication error!!  Selftest terminated =======
    

    2. Connected MSP-GANG to (USB+RS232) and performed Self Test
     → This is because the power is supplied via USB.

    === MSP-GANG Self test results ( Friday, September 24, 2021,  15:34:16 ) ===
    
    Adapter SN ------:  20070444 
    Hardware --------:  G430:  01.05
    Access key ------:  MSP-GANG Programmer 
    Silicon Number --:  588C 886E 1700 1C00
    API Firmware ----:  MSP-Gang   A430:  01.03.04.00
    BOOT Firmware ---:  G430BOOT   B430:  01.00.02.00
    GUI Software ----:  MSP-Gang-GUI   G430:  01.03.04.00
    DLL Software ----:  MSP-Gang-DLL   D430:  01.03.04.00
    
    ================ Test results =============
    
    
    No.       name                   parameter       limits               result         status
    
    
      1: Data Bus   (ALL LOW)          0x0000   (0x0000  - 0x0000)  Result:  0x00     ... >>  OK   <<
      2: Data Bus   (ALL HIGH)         0x00FF   (0xFFFF  - 0xFFFF)  Result:  0xFFFF   ... >>  OK   <<
      3: Data Bus   (D-0 HI )          0x0001   (0x0101  - 0x0101)  Result:  0x0101   ... >>  OK   <<
      4: Data Bus   (D-1 HI )          0x0002   (0x0202  - 0x0202)  Result:  0x0202   ... >>  OK   <<
      5: Data Bus   (D-2 HI )          0x0004   (0x0404  - 0x0404)  Result:  0x0404   ... >>  OK   <<
      6: Data Bus   (D-3 HI )          0x0008   (0x0808  - 0x0808)  Result:  0x0808   ... >>  OK   <<
      7: Data Bus   (D-4 HI )          0x0010   (0x1010  - 0x1010)  Result:  0x1010   ... >>  OK   <<
      8: Data Bus   (D-5 HI )          0x0020   (0x2020  - 0x2020)  Result:  0x2020   ... >>  OK   <<
      9: Data Bus   (D-6 HI )          0x0040   (0x4040  - 0x4040)  Result:  0x4040   ... >>  OK   <<
     10: Data Bus   (D-7 HI )          0x0080   (0x8080  - 0x8080)  Result:  0x8080   ... >>  OK   <<
    
     11: Data-2 Bus  (ALL LOW)         0x0000   (0x0000  - 0x0000)  Result:  0x00     ... >>  OK   <<
     12: Data-2 Bus  (ALL HIGH)        0x00FF   (0xFFFF  - 0xFFFF)  Result:  0xFFFF   ... >>  OK   <<
     13: Data-2 Bus  (D2-0 HI )        0x0001   (0x0101  - 0x0101)  Result:  0x0101   ... >>  OK   <<
     14: Data-2 Bus  (D2-1 HI )        0x0002   (0x0202  - 0x0202)  Result:  0x0202   ... >>  OK   <<
     15: Data-2 Bus  (D2-2 HI )        0x0004   (0x0404  - 0x0404)  Result:  0x0404   ... >>  OK   <<
     16: Data-2 Bus  (D2-3 HI )        0x0008   (0x0808  - 0x0808)  Result:  0x0808   ... >>  OK   <<
     17: Data-2 Bus  (D2-4 HI )        0x0010   (0x1010  - 0x1010)  Result:  0x1010   ... >>  OK   <<
     18: Data-2 Bus  (D2-5 HI )        0x0020   (0x2020  - 0x2020)  Result:  0x2020   ... >>  OK   <<
     19: Data-2 Bus  (D2-6 HI )        0x0040   (0x4040  - 0x4040)  Result:  0x4040   ... >>  OK   <<
     20: Data-2 Bus  (D2-7 HI )        0x0080   (0x8080  - 0x8080)  Result:  0x8080   ... >>  OK   <<
    
     21: Vcc Target-1 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.03 V   ... >>  OK   <<
     22: Vcc Target-2 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
     23: Vcc Target-3 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
     24: Vcc Target-4 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
     25: Vcc Target-5 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
     26: Vcc Target-6 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
     27: Vcc Target-7 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
     28: Vcc Target-8 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
    
     29: Translators VT (OFF)           0.00 V  (  0.00 to   0.50)  Result:  0.01 V   ... >>  OK   <<
     30: Translators VT (ON 1.8V)       1.80 V  (  1.60 to   2.00)  Result:  1.77 V   ... >>  OK   <<
     31: Translators VT (ON 2.7V)       2.70 V  (  2.50 to   2.90)  Result:  2.64 V   ... >>  OK   <<
     32: Translators VT (ON 3.6V)       3.60 V  (  3.40 to   3.80)  Result:  3.51 V   ... >>  OK   <<
    
     33: Vpp Voltage-in                10.00 V  (  8.00 to  12.00)  Result: 10.23 V   ... >>  OK   <<
     34: Vpp Voltage                    7.00 V  (  6.50 to   7.30)  Result:  6.88 V   ... >>  OK   <<
     35: Internal Vcc-3.3V              3.30 V  (  3.20 to   3.40)  Result:  3.30 V   ... >>  OK   <<
    
     36: Vcc Target-1 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.80 V   ... >>  OK   <<
     37: Vcc Target-2 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.83 V   ... >>  OK   <<
     38: Vcc Target-3 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.79 V   ... >>  OK   <<
     39: Vcc Target-4 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.80 V   ... >>  OK   <<
     40: Vcc Target-5 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.80 V   ... >>  OK   <<
     41: Vcc Target-6 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.81 V   ... >>  OK   <<
     42: Vcc Target-7 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.80 V   ... >>  OK   <<
     43: Vcc Target-8 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.79 V   ... >>  OK   <<
     44: Vcc Target-1 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.67 V   ... >>  OK   <<
     45: Vcc Target-2 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.70 V   ... >>  OK   <<
     46: Vcc Target-3 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.67 V   ... >>  OK   <<
     47: Vcc Target-4 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.69 V   ... >>  OK   <<
     48: Vcc Target-5 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.68 V   ... >>  OK   <<
     49: Vcc Target-6 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.69 V   ... >>  OK   <<
     50: Vcc Target-7 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.68 V   ... >>  OK   <<
     51: Vcc Target-8 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.67 V   ... >>  OK   <<
     52: Vcc Target-1 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.55 V   ... >>  OK   <<
     53: Vcc Target-2 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.59 V   ... >>  OK   <<
     54: Vcc Target-3 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.56 V   ... >>  OK   <<
     55: Vcc Target-4 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.57 V   ... >>  OK   <<
     56: Vcc Target-5 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.57 V   ... >>  OK   <<
     57: Vcc Target-6 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.58 V   ... >>  OK   <<
     58: Vcc Target-7 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.56 V   ... >>  OK   <<
     59: Vcc Target-8 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.55 V   ... >>  OK   <<
    
     60: Vcc discharge (100ms)Target-1  3.60 V  (  1.00 to   2.70)  Result:  1.19 V   ... >>  OK   <<
     61: Vcc discharge (100ms)Target-2  3.60 V  (  1.00 to   2.70)  Result:  1.16 V   ... >>  OK   <<
     62: Vcc discharge (100ms)Target-3  3.60 V  (  1.00 to   2.70)  Result:  1.19 V   ... >>  OK   <<
     63: Vcc discharge (100ms)Target-4  3.60 V  (  1.00 to   2.70)  Result:  1.21 V   ... >>  OK   <<
     64: Vcc discharge (100ms)Target-5  3.60 V  (  1.00 to   2.70)  Result:  1.17 V   ... >>  OK   <<
     65: Vcc discharge (100ms)Target-6  3.60 V  (  1.00 to   2.70)  Result:  1.20 V   ... >>  OK   <<
     66: Vcc discharge (100ms)Target-7  3.60 V  (  1.00 to   2.70)  Result:  1.19 V   ... >>  OK   <<
     67: Vcc discharge (100ms)Target-8  3.60 V  (  1.00 to   2.70)  Result:  1.20 V   ... >>  OK   <<
    
     68: Vcc Target-1 ( #1 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.27 V   ... >>  OK   <<
     69: Vcc Target-2 ( #1 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     70: Vcc Target-3 ( #1 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     71: Vcc Target-4 ( #1 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     72: Vcc Target-5 ( #1 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     73: Vcc Target-6 ( #1 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     74: Vcc Target-7 ( #1 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     75: Vcc Target-8 ( #1 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     76: Vcc Target-1 ( #2 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.17 V   ... >>  OK   <<
     77: Vcc Target-2 ( #2 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.29 V   ... >>  OK   <<
     78: Vcc Target-3 ( #2 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     79: Vcc Target-4 ( #2 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     80: Vcc Target-5 ( #2 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     81: Vcc Target-6 ( #2 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     82: Vcc Target-7 ( #2 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     83: Vcc Target-8 ( #2 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     84: Vcc Target-1 ( #3 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     85: Vcc Target-2 ( #3 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     86: Vcc Target-3 ( #3 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.26 V   ... >>  OK   <<
     87: Vcc Target-4 ( #3 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     88: Vcc Target-5 ( #3 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     89: Vcc Target-6 ( #3 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     90: Vcc Target-7 ( #3 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     91: Vcc Target-8 ( #3 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     92: Vcc Target-1 ( #4 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     93: Vcc Target-2 ( #4 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     94: Vcc Target-3 ( #4 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     95: Vcc Target-4 ( #4 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.28 V   ... >>  OK   <<
     96: Vcc Target-5 ( #4 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
     97: Vcc Target-6 ( #4 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     98: Vcc Target-7 ( #4 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
     99: Vcc Target-8 ( #4 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    100: Vcc Target-1 ( #5 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    101: Vcc Target-2 ( #5 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    102: Vcc Target-3 ( #5 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    103: Vcc Target-4 ( #5 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    104: Vcc Target-5 ( #5 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.27 V   ... >>  OK   <<
    105: Vcc Target-6 ( #5 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    106: Vcc Target-7 ( #5 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    107: Vcc Target-8 ( #5 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    108: Vcc Target-1 ( #6 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    109: Vcc Target-2 ( #6 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    110: Vcc Target-3 ( #6 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    111: Vcc Target-4 ( #6 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    112: Vcc Target-5 ( #6 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    113: Vcc Target-6 ( #6 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.28 V   ... >>  OK   <<
    114: Vcc Target-7 ( #6 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    115: Vcc Target-8 ( #6 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    116: Vcc Target-1 ( #7 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    117: Vcc Target-2 ( #7 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    118: Vcc Target-3 ( #7 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    119: Vcc Target-4 ( #7 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    120: Vcc Target-5 ( #7 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    121: Vcc Target-6 ( #7 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    122: Vcc Target-7 ( #7 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.26 V   ... >>  OK   <<
    123: Vcc Target-8 ( #7 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    124: Vcc Target-1 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    125: Vcc Target-2 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    126: Vcc Target-3 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    127: Vcc Target-4 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    128: Vcc Target-5 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    129: Vcc Target-6 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
    130: Vcc Target-7 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
    131: Vcc Target-8 ( #8 ON )         3.30 V  (  3.10 to   3.50)  Result:  3.26 V   ... >>  OK   <<
    
    132: SD Power OFF                  0x0000   (0x0000  - 0x0000)  Result:  0x00     ... >>  OK   <<
    133: SD Power ON                   0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    134: SD Discharge -  delay 2ms     0x0010   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    135: SD Discharge -  delay 50ms    0x0010   (0x0000  - 0x0000)  Result:  0x00     ... >>  OK   <<
    
    136: BSL RX bus (#1 HIGH)          0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    137: BSL RX bus (#2 HIGH)          0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
    138: BSL RX bus (#3 HIGH)          0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
    139: BSL RX bus (#4 HIGH)          0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
    140: BSL RX bus (#5 HIGH)          0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
    141: BSL RX bus (#6 HIGH)          0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
    142: BSL RX bus (#7 HIGH)          0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
    143: BSL RX bus (#8 HIGH)          0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<
    
    144: BSL TX bus (#1 HIGH)          0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    145: BSL TX bus (#2 HIGH)          0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
    146: BSL TX bus (#3 HIGH)          0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
    147: BSL TX bus (#4 HIGH)          0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
    148: BSL TX bus (#5 HIGH)          0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
    149: BSL TX bus (#6 HIGH)          0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
    150: BSL TX bus (#7 HIGH)          0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
    151: BSL TX bus (#8 HIGH)          0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<
    
    152: TDI bus  (#1 HIGH)            0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    153: TDI bus  (#2 HIGH)            0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
    154: TDI bus  (#3 HIGH)            0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
    155: TDI bus  (#4 HIGH)            0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
    156: TDI bus  (#5 HIGH)            0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
    157: TDI bus  (#6 HIGH)            0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
    158: TDI bus  (#7 HIGH)            0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
    159: TDI bus  (#8 HIGH)            0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<
    
    160: TDOI Tx-bus (#1 HIGH)         0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    161: TDOI Tx-bus (#2 HIGH)         0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
    162: TDOI Tx-bus (#3 HIGH)         0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
    163: TDOI Tx-bus (#4 HIGH)         0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
    164: TDOI Tx-bus (#5 HIGH)         0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
    165: TDOI Tx-bus (#6 HIGH)         0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
    166: TDOI Tx-bus (#7 HIGH)         0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
    167: TDOI Tx-bus (#8 HIGH)         0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<
    
    168: TDOI Tx-Rx (#1 HIGH)          0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    169: TDOI Tx-Rx (#2 HIGH)          0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
    170: TDOI Tx-Rx (#3 HIGH)          0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
    171: TDOI Tx-Rx (#4 HIGH)          0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
    172: TDOI Tx-Rx (#5 HIGH)          0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
    173: TDOI Tx-Rx (#6 HIGH)          0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
    174: TDOI Tx-Rx (#7 HIGH)          0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
    175: TDOI Tx-Rx (#8 HIGH)          0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<
    
    176: TDOI Rx-bus (#1 HIGH)         0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    177: TDOI Rx-bus (#2 HIGH)         0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
    178: TDOI Rx-bus (#3 HIGH)         0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
    179: TDOI Rx-bus (#4 HIGH)         0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
    180: TDOI Rx-bus (#5 HIGH)         0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
    181: TDOI Rx-bus (#6 HIGH)         0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
    182: TDOI Rx-bus (#7 HIGH)         0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
    183: TDOI Rx-bus (#84 HIGH)        0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<
    
    184: TMS bus (All HIGH)            0x00FF   (0x00FF  - 0x00FF)  Result:  0xFF     ... >>  OK   <<
    185: TMS bus (All LOW)             0x0000   (0x0000  - 0x0000)  Result:  0x00     ... >>  OK   <<
    
    186: TMS bus (#1 HIGH)             0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    187: TMS bus (#2 HIGH)             0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
    188: TMS bus (#3 HIGH)             0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
    189: TMS bus (#4 HIGH)             0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
    190: TMS bus (#5 HIGH)             0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
    191: TMS bus (#6 HIGH)             0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
    192: TMS bus (#7 HIGH)             0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
    193: TMS bus (#8 HIGH)             0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<
    
    194: RST bus (All HIGH)            0x00FF   (0x00FF  - 0x00FF)  Result:  0xFF     ... >>  OK   <<
    195: RST bus (All LOW)             0x0000   (0x0000  - 0x0000)  Result:  0x00     ... >>  OK   <<
    
    196: RST bus (#1 HIGH)             0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    197: RST bus (#2 HIGH)             0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
    198: RST bus (#3 HIGH)             0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
    199: RST bus (#4 HIGH)             0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
    200: RST bus (#5 HIGH)             0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
    201: RST bus (#6 HIGH)             0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
    202: RST bus (#7 HIGH)             0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
    203: RST bus (#8 HIGH)             0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<
    
    204: Keys buffer (All pull-up)     0x001F   (0x001F  - 0x001F)  Result:  0x1F     ... >>  OK   <<
    
    205: Access to LCD RAM (0xAA)      0x00AA   (0x00AA  - 0x00AA)  Result:  0xAA     ... >>  OK   <<
    206: Access to LCD RAM (0x99)      0x0099   (0x0099  - 0x0099)  Result:  0x99     ... >>  OK   <<
    
    207: Image Flash Access (get ID)   0x0002   (0x0001  - 0x0004)  Result:  0x04     ... >>  OK   <<
    
    208: TDI Fuse keys (#1 ON)         0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
    209: TDI Fuse keys (#2 ON)         0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
    210: TDI Fuse keys (#3 ON)         0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
    211: TDI Fuse keys (#4 ON)         0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
    212: TDI Fuse keys (#5 ON)         0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
    213: TDI Fuse keys (#6 ON)         0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
    214: TDI Fuse keys (#7 ON)         0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
    215: TDI Fuse keys (#8 ON)         0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<
    
    216: TEST Fuse keys (All OFF )      0.00    (  0.00 to   0.30)  Result:  0.00     ... >>  OK   <<
    217: TEST Fuse keys (#1 ON)         1.00    (  0.80 to   3.00)  Result:  1.31     ... >>  OK   <<
    218: TEST Fuse keys (#2 ON)         2.00    (  0.80 to   3.00)  Result:  1.39     ... >>  OK   <<
    219: TEST Fuse keys (#3 ON)         3.00    (  0.80 to   3.00)  Result:  1.49     ... >>  OK   <<
    220: TEST Fuse keys (#4 ON)         4.00    (  0.80 to   3.00)  Result:  1.54     ... >>  OK   <<
    221: TEST Fuse keys (#5 ON)         5.00    (  0.80 to   3.00)  Result:  1.54     ... >>  OK   <<
    222: TEST Fuse keys (#6 ON)         6.00    (  0.80 to   3.00)  Result:  1.48     ... >>  OK   <<
    223: TEST Fuse keys (#7 ON)         7.00    (  0.80 to   3.00)  Result:  1.47     ... >>  OK   <<
    224: TEST Fuse keys (#8 ON)         8.00    (  0.80 to   3.00)  Result:  1.46     ... >>  OK   <<
    
    ============== Finished =================================
    *  Test pass - no errors.
    =========================================================
    

    As a result, it seems that the Self Test is still not performed only by the USB connection in 1) above. However, in case 2) above, the Self Test passed.
    The drivers are up to date, and they have tried several USB cables, but the result is that Self Test still does not work if connect only USB.
    Is there anything else we should check regarding the point that it does not work with USB?

  • Hi Yasutoshi,

    I think this is not the USB wire issue, this should USB driver not install normal, you can check if there are MSP-GANG-CDC port in device manager.

    When you connect USB&RS232, maybe the communication is through RS232, thus you can get self test pass information.

    Thanks!

    Best Regards

    Johnson

  • Hi Johnson,

    The customer finally contacted me with the results of the confirmation, but they said that the situation was the same even after reloading the driver several times. Below is a picture of the confirmation.

    Best regards,

    Yasutoshi

  • Hi Yasutoshi,

    Unfortunately, I don't reproduce this issue in my side.

    And I find you can read the DLL software version in USB and USB+RS232, could you try to check if you can update this firmware via MSP-GANG GUI?

    And just would like to check one thing: This issue only occur this PC? Do you try to another PC? I see you have been tried in two PC(BBC-1010-H7D-W7 & SIMATIC IPC647C), Have you tried a third PC? I just want to confirm that this is a common issue, or just follow this PC.

    Thanks!

    Best Regards

    Johnson

**Attention** This is a public forum