Part Number: MSP430FR2355
Good evening....
I would like to create a HW watchpoint on TB1CCTL1 when the CCIFG gets set....I select watchpoint with Data under breakpoints and enter the register along with write....The question is what hex value do I want to put so that the code stops and the breakpoint triggers when CCIFG goes off? I tried 0x01 but the code doesn't seem to stop ....
I can easily place a HW breakpoint in the ISR but what I would really like to know is prior to getting to the ISR where the code is when the CCIFG goes from 0 to 1 after CCIE has been set
Thanks