This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5510: Judgment timing of PUR pin in USB BSL

Guru 12295 points
Part Number: MSP430F5510


Hi, 

There is a statement in MSP430 USB Hardware Design Guide P.18 that the PUR pin becomes an input and is judged after BOR reset.

1. Is there any information that the judgment will start within seconds after the BOR occurs?

2. How many seconds does the MCU need to be HIGH to recognize the PUR as HIGH?

 

Background of the question
The MCU may or may not recognize the PUR when the HIGH is long or short.  We are investigating the timing when BUR judgment starts from the next waveform.

※This waveform pulls up R45 and intentionally outputs D +.

Thanks,

Koki

**Attention** This is a public forum