This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am trying to implement a neural network model on a MSP430FR5994 - the model will be pre-trained offline and only needs to run on the MCU. The purpose of the project is to capture audio signals - process them through FFT and then once they are passed through the model - the resultant code needs to be uploaded back to the MCU.
I have already managed to convert some sample keras models into C files which contain the weights and biases of the neural network used to process the signals. Since this is my first time working with the MSP430, I am not exactly sure how these C files which contain the weights can be uploaded onto the MCU. One method that I was considering included a converter called - keras2c - which processes the entire model and then generates a complete C executable file - the resultant header and C files could be loaded into the MSP as a library which could be used for the project.
While seaerching across the forum for similar questions, I found a thread that mentions uploading the pre-trained model into the FRAM of the MCU - however, I am not completely clear about this process and would highly appreciate if I could get a bit more details or clarity about this method.
If there is any more information needed to clarify the understanding of the issue, please feel free to write so in the replies as this is my first question on the forum - I would gladly update the thread accordingly.
Hi Siddhant,
I would recommend that you check out the MSP430 Fundamentals Workshop for CCS [link]. This goes over using the Code Composer Studio (CCS) environment on an MSP430 Launchpad.
For uploading standard C files to the MCU, I would look at section 6.1.2.2. "Adding or Linking Source File to Project" of the CCS User's Guide [link].
Thanks,
Urica Wang
**Attention** This is a public forum