This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5438: Error while Programming MSP430F5438 using BSL method

Part Number: MSP430F5438


Hello,

 

I am trying to program MSP430F5438 using BSL programming. Using BSL_Scripter for the same. But it failed to program. Referring MSP430Tm Flash Devices Bootloader (BSL) SLAU319AE & BSL Scripter document.

In hardware, using FT232H USB module which is acting as COM port connections are as below:

 

                MSP430 Pins                                                    FT232H Pins

RST/NMI/SBWTDIO Entry sequence signal                  DTR

TEST/SBWTCK Entry sequence signal                         RTS

P1.1 BSL Data transmit                                                  RxD

P1.2 BSL Data receive                                                   TxD

VCC Power supply                                                          3.3V

VSS Ground supply                                                         GND

 

Here is my BSL script:

MODE 543x_family UART COM17 PARITY

VERBOSE

MASS_ERASE

RX_PASSWORD

RX_DATA_BLOCK testmspnew.txt

 

 

Errors are as below:

C:\Users\USER\Desktop\MSPTEST>BSL_Scripter.exe Script2.txt

---------------------------------------------------------

BSL Scripter 3.2.1

PC software for BSL programming

2021-Nov-20 13:01:46

---------------------------------------------------------

Input file script is : C:/Users/USER/Desktop/MSPTEST/Script2.txt

MODE 543x_family UART COM17 PARITY

        Baud rate setup for UART is not given / wrong

        It will be setup to the default 9600baud

VERBOSE

        Verbose mode is now on!

MASS_ERASE

        [80] [01] [00] [15] [64] [a3]

        [ACK_ERROR_MESSAGE]Unknown ACK value!

RX_PASSWORD

        [80] [11] [00] [11] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff]

        [ff] [ff] [ff] [ff] [4e] [c9]

        [ACK_ERROR_MESSAGE]Unknown ACK value!

RX_DATA_BLOCK testmspnew.txt

        Read Txt File  : C:\Users\USER\Desktop\MSPTEST\testmspnew.txt

        [80] [1e] [00] [10] [00] [5c] [00] [81] [00] [00] [5c] [b1] [13] [30] [00] [0c]

        [43] [b1] [13] [00] [00] [b1] [13] [2a] [00] [32] [d0] [10] [00] [fd] [3f] [03]

        [43] [ba] [f6]

        [ACK_ERROR_MESSAGE]Unknown ACK value!

        Time elapsed of writing 26 bytes : 1.42 seconds

        Speed of writing data :0.01788(kB/s)

 

C:\Users\USER\Desktop\MSPTEST>

 

Help in this, Thanks in advance.

**Attention** This is a public forum