This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6724: Problems with duplicated serial numbers

Part Number: MSP430F6724

Greetings,

I've read some threads in this forum, about the serialization of devices by using the MSP Gang programmer.

We're facing the same issue in our laboratory, where we program some TI microcontrollers by adding a serial number to the FW.

This serial number has to be unique for wach device, however from time to time some of them are duplicated.

The main issue is due to to fact that the application doesn't give any indication if a serial number is duplicated.

We realise this by checking the log at the end of the operation, however it's too late because maybe we duplicated serial numbers #99 and #100 out of 200 devices.

This is what we use:

- MSP Gang Programmer HW name: G430

- Revision 01.04

- API FW in MSP-Gang: 01.03.03.00

Did anybody ever encounter a similar issue?

Thanks,

best regards,

Gischio

**Attention** This is a public forum