Part Number: MSP430FR6979
Other Parts Discussed in Thread: UNIFLASH,
Hi experts,
My customer is using UniFlash to write to the MSP430FR6979 and is having problems.
- OS: Win10
- UniFlash: v6.4.0, v7.0.0
[1.Error when writing]: "Cannot read property 'DS' of undefined".
Q1:Could you tell me the countermeasure and cause for this error?
They tried uninstalling UniFlash, restarting the PC, and reinstalling(v6.4.0 and v7.0.0) it, referring to the following thread, but it didn't help.
https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/781581/awr1642boost-uniflash--cannot-read-property-ds-of-undefined
When they starts UniFlash with the network connected, the above error occurs when writing. If they turn off the network and start up UniFlash, it writes normally. (If it connect the network after starting UniFlash, it will work correctly, so something is communicating at the start-up timing...?)
[2.About the verification error]: "MSP430: File Loader: Verification failed: Values at address 0x4420 do not match Please verify target memory and memory Please verify target memory and memory map.]
They are checking with reference to the following URL.
:https://software-dl.ti.com/ccs/esd/documents/troubleshooting-data_verification_errors.html
:https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/805617/msp430fr6879-uniflash-program-verification-fails-after-power-cycle
Q2:Please let me know if there are any other priorities that I should check.
Best regards,
O.H