Other Parts Discussed in Thread: MSP-FET
Hi,
We are using MSP430fr5734 and are trying to flash it using Spy Bi Wire interface from MSP430-FET.
The connections are as follows:
1. On board VCC_3V3 -> VCC_Target of MSP-FET
2. GND -> GND of MSP-FET
3. TEST -> TCK of MSP-FET
4. RST -> TDI/TDO of MSP-FET
We are unable to flash the device. The resistor and capacitor at RST pin are as specified in the datasheet.
Is this because of password protection?
Is so, what is the default password to be entered into the target configuration file?