Other Parts Discussed in Thread: MSP430G2302
Hi,
We have built a customized board with MSP430G2302 and the board has its own power supply. The debugging connection was designed to be Spy-Bi-Wire.
We followed the 2-wire connection scheme in http://processors.wiki.ti.com/index.php/JTAG_(MSP430). However, CCS gave us “Error connecting to the target: Unknown device” error.
After comparing the schematics with ours, we noted that we missed the 47Kohm R1, 2.2nF C1 and the 330ohm R2. We could do some jump wiring quickly to add these connections to the board however the board space is limited. So which of these missed wires components are imperative? I guess R1?
We also have some questions for the 2-wire schematics. Footnote B says that C1 has 2.2nF upper limit. Isn’t the larger the better?
Footnote C says when fuse blow is not used, R2=0 and “connection TEST/VPP must not be made”, and this expression is quite confusing. Does it basically mean that if fuse blow is not needed, TCK and the TEST/VPP network should be disconnected?
The last question is that in CCS’s target configuration we found no option toggling 2-wire or 4-wire connection. So does MSP-FET430UIF detect 2-wire/4-wire automatically?
John