Part Number: CCSTUDIO-MSP
Hello, I am having the same issue as everyone on this thread. Could you please share your solution with me?
I'm also running Windows 11
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CCSTUDIO-MSP
Hello, I am having the same issue as everyone on this thread. Could you please share your solution with me?
I'm also running Windows 11
Thanks
Hi,
Thanks for the fast reply. Here's the screenshot of the error I'm getting.
Seems to be the same as in the original thread.


From the install logs:
Certificate "VeriSign Class 3 Public Primary Certification Authority - G5" already in store.
Related Certificates:
Exact match:
Element 0:
Serial Number: 39ad63d2f5c9efdc46d734ae5e381b8f
Issuer: CN=VeriSign Class 3 Code Signing 2010 CA, OU=Terms of use at https://www.verisign.com/rpa (c)10, OU=VeriSign Trust Network, O=VeriSign, Inc., C=US
NotBefore: 2/25/2014 4:00 PM
NotAfter: 2/25/2017 3:59 PM
Subject: CN=Texas Instruments Incorporated, OU=Digital ID Class 3 - Microsoft Software Validation v2, O=Texas Instruments Incorporated, L=Dallas, S=Texas, C=US
Non-root Certificate
Cert Hash(sha1): ee0c8ba018ce926432c3cc23523a34073d01954a
Certificate "Texas Instruments Incorporated" already in store.
CertUtil: -addstore command completed successfully.
Script stderr:
Executing C:\ti\ccs1020/ccs/ccs_base\emulation\drivers\msp430\DPInst\DPinst64.exe /q /se /sa /lm /path "C:\ti\ccs1020/ccs/ccs_base\emulation\drivers\msp430\USB_eZ-RF"
Script exit code: unknown signal
Script output:
Script stderr:
child killed: unknown signal
Error running C:\ti\ccs1020/ccs/ccs_base\emulation\drivers\msp430\DPInst\DPinst64.exe /q /se /sa /lm /path "C:\ti\ccs1020/ccs/ccs_base\emulation\drivers\msp430\USB_eZ-RF": child killed: unknown signal
[14:53:31] dpinst return code = unknown signal
Thanks
Hi Juan,
You are install the old version V10.2. Download and try to install the last version V11.1.0.
**Attention** This is a public forum