Other Parts Discussed in Thread: MSP430F2013
Hi Team,
This inquiry is a continuation of the other thread. According to our customer,
Thank you for your assistance, I am searching for an example code for transferring data from SD16MEMO to USI on MSP430F2XX but I am not successful enough till so can you please point me towards an example here.
Here is my code which I was able to piece together while searching some examples and from other members' query requests
#include <msp430.h>
/* Arrays to store SD16 conversion results */
/* NOTE: arrays need to be global to */
/* prevent removal by compiler */
static volatile unsigned int ChA0results = 0x00;
static volatile unsigned int ChA1results = 0x00;
static volatile unsigned int ChA2results = 0x00;
static unsigned int ch_counter=0;
int main(void)
{
volatile unsigned int i; // Use volatile to prevent removal
// by compiler optimization
WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer
BCSCTL1 = CALBC1_16MHZ;
DCOCTL=CALDCO_16MHZ;
P1OUT |= BIT5;
P1DIR |= BIT5;
P1DIR |= 0x10; //P1.4 as output
P1SEL = 0x10; //SMCLK to P1.4
P1DIR |= BIT7; //set P1.7 to output direction - as signal for data are ready to us
SD16CTL = SD16REFON + SD16SSEL_1; // 1.2V ref, SMCLK
SD16INCTL0 = SD16INCH1; // Set channel A0+/-
SD16CCTL0 |= SD16SNGL + SD16UNI + SD16IE;
// Single conv, 256OSR, unipolar,
// enable interrupt
SD16INCTL0 |= SD16INTDLY_0; // Interrupt on 4th sample
SD16AE = SD16AE1; // P1.0 A0+, A0- = VSS
USICTL0 &= ~USISWRST; //USI released for operation
USICTL1 &= ~USII2C; //switch USI to SPI-Mode
USICTL0 &= USIMST; //set to SPI-Slave-Mode
USICTL0 |= USIPE5; //SCLK as input (from Warrior56)
USICTL0 |= USIPE6; //SDO-Port enabled; Pin8
USICTL0 &= ~USIPE7; //SDI-Port disabled; Pin9 can be used for normal in/out
USICTL0 |= USIOE; //activate output (data goes from MSP to Warrior56)
USICNT |= USI16B; //init load counter for 16-bit-data
//inactive state is low
//data is changed on the first SCLK edge and captured on the following edge
for (i = 0; i < 0x3600; i++); // Delay for 1.2V ref startup
while(1)
{
SD16CCTL0 |= SD16SC; // Set bit to start conversion
__bis_SR_register(LPM0_bits + GIE); // Enter LPM0
}
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = SD16_VECTOR
__interrupt void SD16ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(SD16_VECTOR))) SD16ISR (void)
#else
#error Compiler not supported!
#endif
{
ChA0results = SD16MEM0; // Save CH0 results (clears IFG)
SD16AE &= ~SD16AE1; // Disable external input A0+, A0
SD16INCTL0 &= ~SD16INCH_1; // Disable channel A0+/-
ch_counter++;
USISR = SD16MEM0;
SD16INCTL0 |= SD16INCH_1; // Enable channel A1+/-
SD16AE |= SD16AE2; // Enable external input on A1+
}
Regards,
Danilo