This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm installing CCS on win11. I got the following errors: ccs_setup_11.1.0.00011.exe
Already send the diagnose data.
Thanks,
Jinsheng
It works fine for me for the updated 430G2 launchpad, not the old one. There is no problem with serial communication on the Mac.
You mean you are using MSP-EXP430G2ET ? I'm using the old model MSP-EXP430G2 REV1.4 board. It uses TIUSB3014+MSP430F1612 as on-board JTAG debugger. The old one does't work on MAC, right?
Hello Jason,
This older debugger on the older G2 Launchpad is no longer supported in the newer CCS versions. For the best experience, it is recommended to update your EVM to the newer MSP-EXP430G2ET . The main difference is the upgraded debugger circuit that gets you debug features inline with the rest of the Launchpad ecosystem, including EnergyTrace.
**Attention** This is a public forum