This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-FR6043: EVM430-FR6043

Part Number: EVM430-FR6043


Dear TI,

Good morning!

Please help me to find out the solution of below problems.

1) "DToF -shift was greater than maximum sample shift" 

This above error is displaying again and again. Please help me to overcome this issue.

Although, I have been tried to change the "USS_ALG_MAX_SAMPLE_SHIFT " value from 20 to 40 in source code header file " USS_userconfig.h "  to escape this error. 

2) My flow tube is L-shaped and have one reflective surface inside the tube. I have used Audiowell 200KHz ultrasonic transducers and propagation length between both the transducers is ~135mm.

    Please help me to overcome the issue of instability of volume reading on EVM6043 and also the ADC value as shown below figures.

**Attention** This is a public forum