Part Number: EVM430-FR6047
Other Parts Discussed in Thread: TIDA-01486, EVM430-FR6043
Hello team,
I was working on an testbed solution with EVM430-FR6047, that seemed to work well.
After moving to a real water pipe (diameter 90mm and wall thickness 8mm) I can't make it work.
By changing the parameters the AC Capture seemed somehow ok, the sensor doesn't get the different when water is flowing or not.
I am wondering If I should use use also an amplifier like TIDA-01486
Can someone help?
Thanks in advance