This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP430G2: Launchpad not working anymore

Part Number: MSP-EXP430G2
Other Parts Discussed in Thread: TUSB3410, MSP430F1612,

Hello!

I have a MSP-EXP430G2 Launchpad board (eZ430) and it stopped working.


It was without use during about 1 year and when I tried to use now and connected the cable in PC, the board was not recognized and is not enumerated as USB device.

I was looking in the forum for similar issues and didn't find a solution.

I inspect the board and stated that the 12MHz clock is working from MSP430F1612 to TUSB3410 and the voltage in pin 9 (RESET) of TUSB3410 is about 3.4V.

I did another test: I connected VCC to the pin 5 (PUR) of TUSB3410 and then the board was recognized as USB Device (TUSB3410 Boot Device) as shown bellow. But when I disconnect VCC from pin 5 the USB disconnect.

[15342.637227] usb 1-1.1: new full-speed USB device number 20 using ehci-pci
[15342.763828] usb 1-1.1: New USB device found, idVendor=0451, idProduct=3410, bcdDevice= 1.00
[15342.763844] usb 1-1.1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[15342.763850] usb 1-1.1: Product: TUSB3410 Boot Device
[15342.763854] usb 1-1.1: Manufacturer: Texas Instruments
[15342.763858] usb 1-1.1: SerialNumber: TUSB3410         
[15342.765444] ti_usb_3410_5052 1-1.1:1.0: TI USB 3410 1 port adapter converter detected
[15342.767113] ti_usb_3410_5052 1-1.1:2.0: TI USB 3410 1 port adapter converter detected
[15342.767340] usb 1-1.1: TI USB 3410 1 port adapter converter now attached to ttyUSB0
[15347.131245] usb 1-1.1: USB disconnect, device number 20
[15347.131735] ti_usb_3410_5052_1 ttyUSB0: TI USB 3410 1 port adapter converter now disconnected from ttyUSB0
[15347.131781] ti_usb_3410_5052 1-1.1:2.0: device disconnected

I think it can be caused by corrupted firmware in the EEPROM or in the MSP430F1612.

Someone had the same issue? There is a way to fix it?

Regards,

Luan

**Attention** This is a public forum