This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is is possible to Power the MSP430 with the MSP-FET programmer. I can get my device program when it's powered externally, but it would be more convenient if MSP-FET provided the 3.3V. I'm using the the UniFlash Tool and didn't see that as an option. Thanks!
Hi Justin,
I believe this should just work if you connect VCC_TOOL to your devices power rail instead of VCC_TARGET. Figure below taken from the MSP Debuggers Guide
Regards,
Evan
**Attention** This is a public forum