Other Parts Discussed in Thread: MSP430F2112, , MSP-FET, MSP-TS430PW28, BQ76925EVM, MSP430F2122
Hello, we are moving into production with our MSP430F2112 code and have exported the txt hex file from Code composer. We are using FW V1.03.06.00 for the MSP-GANG programmer and are having issues flashing the code. We are getting ERROR 33: IR communication failed. We're using a custom board with 3.3V VCC voltage. We have a 47k pullup and 2.2nF cap to ground on pin 5 (reset). They are located physically close to the MCU (~1cm away).
We're using this adapter:
https://www.tag-connect.com/product/spy-bi-tag-spy-bi-wire-adapter
with R1 populated and this connector:
We are using an MSP-FET with no issues. We can debug just fine with the MSP-FET. We have tried other ports on the MSP-GANG and have the same issue. Do you have any suggestions? Please let me know if you need any additional information.
Thank you!