This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to program MSP430I4020 chip using MSP430F5529. My device connections are as follows;
3.3V - 3.3V
GND - GND
SBWTST - SBWTST
SBWRST - SBWRST
I tried to code over Uniflash and CCS but I am getting the following error. Is it not possible for me to program the MSP430I4020 chip through another kit?
MSP430: File Loader: Verification failed: Values at address 0xC000 do not match Please verify target memory and memory map.
MSP430: GEL: File: C:\Users\SAKACI\workspace_v9_2\TestMSP2040I\Debug\TestMSP2040I.out: a data verification error occurred, file load failed.
Please set the no verification and see if this can do some help:
**Attention** This is a public forum