This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Our customer is looking for a non-invasive ultrasonic flow-bubble sensor with the following specifications.
Our product requirements:
-Non-Invasive must be
-Should measure the liquid flow(blood)
-Should be able to detect bubbles
-We will use 4 or 2 piezo sensors
-The pipe diameter where the measurement will be made will be a maximum of 1 inch
Our request from you in this regard:
-Which ULTRASONIC FLOW CONVERTER of your company would you recommend us to use?(3501-3503 etc.)
td-sonoflow-co-56-en-sonotec.pdf
-Is an opamp necessary in the circuit we will set up?
-Which microcontroller should we choose?
-And what are your other different suggestions?
Is our ultrasonic sensing solution such as EVM430-FR6047 capable of measuring blood and bubbles?
Regards,
Danilo
Hi Danilo,
MSP430FR6047 be able to measure flow rate for liquid, but I don't think this solution be able to detect bubbles.
Thanks!
Best Regards
Johnson
**Attention** This is a public forum