Part Number: MSP430FR2433
Hi,
I have a GPIO pin which is configured input with a programed pull down.
I'd like to ask what will happend if i give an input voltage more than Vcc+0.3 with Vccmax=3.2V.
There are internal protection in the GPIO? Because i feel that whatever the input voltage, i get only 4V at the GPIO pin.
Thank you
Best regards.
Liang