Other Parts Discussed in Thread: TMS320VC5509A
The differences between the microstar and nfbga packages for the products are primarily mechanical (specifically a minor height difference). The key parameters for the two packages are the same. The paths for the nfbga package substrate was designed to enable the parts to be considered datasheet equivalent (share the same datasheet; and power, ground and signal pins are all in the same X-Y locations).
Board Layout Considerations:
The nFBGA package provides the same X and Y dimensions as MicroStar BGA, and provides pin-to-pin and footprint compatibility. Minor adjustments in pick and place machine programming may be needed because of slight package and tray differences. The nfBGA package can solder to the Microstar BGA land pattern. However, there have been improved nFBGA PCB land pattern and stencil recommendations to achieve better soldering results after extensive testing and evaluation since the microstar package was developed. Please refer to the latest TI packaging drawing found in the latest TI device datasheet and datasheet addendum to review the package dimensions and latest PCB land pattern and stencil recommendation. For more details, check out this nFBGA application note*
*Note: I looked into the nFBGA packaging application report and did not find anything on the 5 x 5 mm x 0.5mm pitch package which is not helping me... (https://www.ti.com/lit/an/spraa99c/spraa99c.pdf?ts=1666997354717&ref_url=https%253A%252F%252Fe2e.ti.com%252F)