Part Number: MSP-EXP430F5529LP
Other Parts Discussed in Thread: TDC7200EVM, , TDC7200
To evaluate TDC7200 performance, the only TDC7200 evaluation board I can get is TDC7200EVM. To run it has to have MSP-EXP430F5529LP (according to user's guide). As connect two boards and start TDC7200EVM software, it shows " Connect Failed! Check hardware. Exiting...", but com3 & com4 can appear in "Serial Port (I/O)" window. Therefore, I cannot update firmware making LP connection to 7200EVM, and fault to run TDC 7200 evaluation.
1. What's my missing here?
2. I only have CCS Version: 12.2.0.00009 , not IAR. Am I able to run any example project came with "MSP430WARE", cause example projects I've seen in this package are *.eww which id IAR project.
3. If I'm wrong in Q2, which example should I pick to run TDC7200 evaluation then?