Part Number: EVM430-FR6047
Other Parts Discussed in Thread: TDC1000
Hi,
I was attempting to use this dev board to test the accuracy of the MSP430 using just a single 1MHz transducer to get the absolute TOF. I have tried hooking up the transducer to CH1 and then grounding CH2 but that did not seem to work. If anyone has some guidance that would be greatly appreciated.


parameters and have included my settings as well. Unfortunately I am not getting any ADC reading or anything on the waveform graphs. NOTE: Although there are multiple transducers mounted to the bottle I am currently using the one mentioned 


I was taking another look at my ADC capture and saw this but there is a repeating error for "No Signal Detected Upstream"