I had a project to use the MSP432P401R and the color touch screen to drive some stepper motors.
Obviously, I can't use the MSP432 anymore, so what would be the best MSP430 to drive this?
One with a LaunchPad is preferable.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I had a project to use the MSP432P401R and the color touch screen to drive some stepper motors.
Obviously, I can't use the MSP432 anymore, so what would be the best MSP430 to drive this?
One with a LaunchPad is preferable.
Hey Keith,
Your best option is probably the MSP-EXP430F5529LP. I see some discussion on this E2E thread saying there is an example for F5529 in the MSP-GRLIB graphics library.
Hope this can meet your needs.
JD
That looks very interesting. The Dual USB on the launch pad is a bit confusing, though.
**Attention** This is a public forum