This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2272: Grace 3 download link in v6? or CCS App center in v12?

Part Number: MSP430F2272


Dear support team at TI,

I have received the firmware code for one of the sensor we use which s based on the MSP430F2272, I did not developpe the code myself but investigated a bit in the forum and apparently it was made with grace 3.

And I get this error message when I compile with CCSV12

**** Build Finished ****
Buildfile generation error occurred..
Product com.ti.sdo.grace v3.0.1.59 is not currently installed and no compatible version is available. Please install this product or a compatible version.
Build stopped..

I don't want to change the configuration nor really use grace since the board will not change, I just want to do some changes to the UART protocol which is used to communicate the sensor data.

So can I somehow workaround it and not use grace (provided the grace generated code already exists and is presumably part of the project?? 

Also I can't find a way to download the v3.0.1.59 version of grace anywhere.

In v12 the "CSS App center" is not working (down?) at least since Thursday.. I removed the firewall but it seems I still can't connect

I then tried installing CCS v6 (which is presumably the last version supporting grace V3.... and the "CSS app Center" opens bu it doesn't seem to have Grace.. 

So I looked in the CCS v6 Ressource explorer but there also it can't connect to the cloud...

Finally I'll need a way to flash and debug the new image to the msp430 and I noticed the new MSP430 FET programmer (version 2) only seems to work from CCS v7.. so do I need a version 1 and where can I get one?

thank you in advance,

**Attention** This is a public forum