I would like to save a 34K byte image into the 256K FRAM but my compiler gives the following error:
line 169: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. placement with alignment fails for section ".cinit" size 0x68d9. Available memory ranges:
I have never encountered a 'trampoline' or the Cinit before.
I am guessing i am crossing some kind of page boundary?
Is it possible to store an array of 34K bytes?
I created my buffer like this
#pragma SET_DATA_SECTION ( ".fram_vars") // Tell the compiler to put the buffer in FRAM
unsigned char display_buffer[33808] = {..........................data,data............}
Could you help or point me to some literature that can explain what to do please?
Thanks