Part Number: MSP430I2020
Hi TI team,
This is regrading Single Phase Energy Meter Design with RS-485 communication.
We are planning to use MSP430I2020 Metering MCU for the same.
I need your support in reviewing the neutral connection & Ground portion wrt MCU ADC.
Pls review with the below notes..
Note 1: There is a bridge rectifier in between Neutral_IN & GND (So Metering MCU GND & Neutral are same)
Note 2 : AGND & GND are short
Is that ok if Neutral & AGND/GND are diffreent ??
If not OK, pls suggest the power supply ckt.