This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts,
I am posting this on behalf of the customer.
I just need to confirm “MSP430F6736A” The Max clock on Xin for this IC. is only 32.768KHz Yes or No?
And Can I use Higher like 4 Mhz for Xin so that I can achieve 1Mbps Baud Rate at the output ( Based on your Calculator based on yr link below)
At the moment, I am evaluating all the different processors. If The answer is No, Then I have to use another Processor to meet my system requirement of 1 Mbps or higher.
Is there any recommendation?
Best regards,
Jonathan
Hello,
Yes, the max clock on XIN is 32.768 kHz. However, the maximum UART baud rate on this device is 5 Mbaud, which should be more than enough for your application. You would use the DCO instead of an external crystal.
Thank you,
Susan
**Attention** This is a public forum