This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Cant' get UART to transmit correctly at 9600 BAUD when using an external 32Khz clock

Other Parts Discussed in Thread: MSP430F247

I have used the same code many times to set up the UART0 at 9600. when using a crystal tied to xin/xout. Now i'm using a MSP430F247 with an external 32Khz clock tied to XIN only. The UART receives data okay at 9600, but when I transmit I get all 0's or all ones?  I looked at P5.6(ACLK) and it is at 32KHZ. Am i missing something?.

I use this code to set up the UART.

BCSCTL3=XT2S_3+LFXT1S_3; //clock set up

P3SEL = 0x30; // all pins of PORT3 dio except 4,5 are usbtxrx
P3DIR = 0xF7; //ALL OUT EXCEPT P3.3,4,5 usb
P3OUT = 0xCE;



UCA0CTL1=01;//reset as puc
UCA0CTL1 |= UCSSEL_1; // CLK = ACLK
UCA0BR0 = 0x03; // 32kHz/9600 = 3.41 use 3
UCA0BR1 = 0x00; //
UCA0MCTL = UCBRS1 + UCBRS0; // Modulation UCBRSx = 3
UCA0CTL1 &= ~UCSWRST;



**Attention** This is a public forum