This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6749A: Increase Accuracy for Energy Meter calibration for phase.

Part Number: MSP430F6749A

These are the accuracy values after phase calibration. Calibrated at 240V, 10A and 60 degree leading phase angle. And the accuracy for current varying from 1 to 100, the  results are in the below attached image for 0.5 leading, unity pf and 0.5 lagging.

**Attention** This is a public forum