Part Number: MSP430I2020
Other Parts Discussed in Thread: UNIFLASH, MSP430I2040, CCSTUDIO, MSP-FET
hello
i'm trying to flash an MSP430i2020 (and MSP430i2040) but keep getting 'verification failed' when flashing with ccstudio and uniflash
* ccstudio V12
* example blink (via new project.. no changes where made)
* pcb is breadboard with mcu soldered on an adapter board for TSOP28
wat are the minimal requirements (shema) for flashing this mcu via SBW and MSP-FET
current connections
VCC - 10uF and 0.1uF to GND
AVSS - GND
ROSC - GND
DVSS - GND
RST/SBWTDIO - 47k to VCC and 1nF to GND
connection to MSF-FET
1. TDO/TDI -- RST/SBWTDIO
2. VCC_TOOL -- VCC
5. TMS -- TEST/SBWTCK
7. GND -- GND
any feedback is helpfull, i've already designed a pcb but would like to make sure the design is programmable