Part Number: EVM430-FR6043
Hi: I'm using the MSP430-FR6043 , and I have a question about the signal sampling frequency.
Currently , it seems set to 1 MHz, and if I hover over the "signal sampling frequecny" box, I see a table showing the various signal sampling frequencies, for the 80 MHz HSPLL.
I see if I can set the OSR to 160, the signal sampling rate will be 500 KHz..
The question is, how can I get a 500 KHz signal sampling rate ? I see the "Oversampling Rate box" is greyed out, I cant change it to 160.
Please advise any comments,
regards,
Doug