This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello All,
I am trying to program a custom board which has an msp430g2553. I am using CCS Version: 4.2.4.00033, windows 7, x86 OS.
The problem I am having is, I cannot load the program to the msp430g2553.
I am using SPY by wire to load the code.
This is what happens when I try to debug.
There's a communication problem of some sort. maybe too much capacitance on the RST pin, or not enough supply voltage (during programming, a higher voltage is required than for operation, also the current consumption has peaks of some mA)
Hi,
I'm trying to program a custom board too. I have MSP430G2553 in 28 pin version. If I connect it with TI LaunchPad (rev.1.4), it shows "Device not connected or supported". I'm using CCS 5.3.0. Can be the problem I have 47k resistor and 10nF capacitor on RST pin?
Thank you for your answers!
MSP430G2553 is not supported by Launchpad v1.4. You must update Launchpad firmware.
http://processors.wiki.ti.com/index.php/MSP430_LaunchPad_Firmware_Update
MSP430G2553 have same flash parameters like any other MSP430F2xx device, and my programmer don't have any problem with MSP430G253
D:\msp430>flash -f sbw_test_16.hex -e -w -v
File "sbw_test_16.hex"
16384 bytes
Get Device
Device: 0 JTID: 89 Fuse: OK 0FF0: 25 53 0FFD: 01 00
Device: 1 JTID: 89 Fuse: OK 0FF0: F2 27 0FFD: 01 04
Device: 2 JTID: 89 Fuse: OK 0FF0: 25 53 0FFD: 01 00
Device: 3 JTID: 89 Fuse: OK 0FF0: F2 27 0FFD: 01 04
Erase
Write
Address: 0C000 Words: 2014
Address: 0CFBC Words: 2014
Address: 0DF78 Words: 2014
Address: 0EF34 Words: 2014
Address: 0FEF0 Words: 136
Size: 16384 bytes Time: 359 ms Speed: 44,57 KB/s
Verify
Address: 0C000 Words: 8192
Size: 16384 bytes Time: 78 ms Speed: 205,13 KB/s
Release Device
Total Time: 547 ms
D:\msp430>
Hi Dalibor,
Dalibor Sisak said:Can be the problem I have 47k resistor and 10nF capacitor on RST pin"
Yes. For SBW, the capacitor on RST must not exceed 2.2nF. Please see the hardware tool's user's guide diagrams in section 2: www.ti.com/lit/pdf/slau278
For a quick test you could try simply removing the cap and see if you can now program. If you still have issues, it is a good idea to post the section of your schematic that shows your programming connections.
Regards,
Katie
I tried to find and solve software problems, but forgot fix this. Thank you very much Katie, it finally works. :)
**Attention** This is a public forum