This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Our circuit board uses an XT1 crystal (32768 Hz) that not stable in the first 600 ms after the DVCC is applied.
Configuration:
ACLK: XT1CLK
SMCLK:DCOCLKDIV With FLL XT1CLK reference clock
MCLK:DCOCLKDIV With FLL XT1CLK reference clock
Clock status:
OFFG = 1
XT1LFOFFG = 1
So during this time within 600 ms (the crystal not stable) the Fail-Safe Operation will do automatically, right?
Does the fail-safe clock always work correctly (100 %)?
Shall we manually configure the FLL reference clock to REFOCLK during this time (start up) and then switch to the XT1 after the crystal stable (600 ms)?
Hi Tink
May I know the reason of XT1 crystal not stable 600 ms after the DVCC is applied?
from the UG description,
a crystal fault automatically causes the FLL reference source, FLLREFCLK, to be sourced by the REFO.
Hi,
for 600 milliseconds is characteristic of the crystal oscillator circuit. After supplying voltage from 0 V to 3.3 V
I also have some experiments on clock failure states with some conditions of DVCC and AUXVCC1 below.
1) When connecting and disconnecting the DVCC 0 to 3.3 V power supply, connect AUXVCC1 to 3.3 C continuously.
Result: No oscillator failure detected.
2) When connecting and disconnecting the DVCC 0 to 3.3 V power supply, connect AUXVCC1 to 1.4 V and below.
Result: Oscillator failure detected.
Why is an oscillator failure detected (OFFG = 1
XT1LFOFFG = 1) with AUXVCC1 voltage 1.4 and below?
From all of the above my discussion was about suspected cause (clock source failure) of the problem. Where I found the MCU get stuck (the device not start) in the actual use field. But it cannot be reproduced in a laboratory.
This cannot use the debugger to debug where the code is stuck. (becuase the debugger reset the program counter)
Symptoms of the bug were just checked with the H/W pin
(device does not start).
Vcore pin = 1.42 V (core level 0 AM)
Reset pin = 3.3 V
some related issues i discussed.
Hi,
I have another question about code below?
int _system_pre_init(void) { /* Insert your low-level initializations here */ __disable_interrupt(); WDTCTL = WDTPW+WDTHOLD; // Clear RTCHOLD Bit after reset RTCCTL0_H = RTCKEY_H; // unlock RTCCTL1 &= ~RTCHOLD; // release RTC RTCCTL0_H = 0x00; // lock }
Is it correct to clear RTC hold bit in system_pre_init?
Are there any problems/risks when the RTC hold bit is clear in system_pre_init (DVCC and crystal are not yet stable, related to MCU stuck or not)?
Hi Tink
These is _disable_interrupt () at the beginning of the code.
I think all interrupt is disable here.
I don't have idea how to release RTC here because the interrupt is disable
Thanks
**Attention** This is a public forum