Part Number: MSP430FR6043
Hello forum,
had tried for adc capture but i didnt get graph for delta,absolute tof and volume as well as for the frequency sweep...there no graph is produced for these parameters kindly check this asap pls






This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430FR6043
Hello forum,
had tried for adc capture but i didnt get graph for delta,absolute tof and volume as well as for the frequency sweep...there no graph is produced for these parameters kindly check this asap pls






i need the detailed explanation for envelope crossing threshold ,start ppg count ,turn on adc count ,start ppg and in bias count ,external amplifier
tion for
Hi,
For 200kHz transducer, it is recommended to start with F1 170kHz and F2 230kHz at the beginning to test with. Your current configuration is F1 150k and F2 152k, it will cause the library keeps reporting error.
For the meaning of those parameters, please refer to this academy. https://dev.ti.com/tirex/explore/node?node=A__AURAjHTDa0oVdd-2UTgIEQ__MSP430-ACADEMY__8HaEUeq__LATEST
Best regards,
Cash Hao
Hello forum,
by changing the parameter i have got graph as 



kondly check this for get an perfect adc graph
Hi,
A lower gain setting is preferred, it will lower the DC offset. Keep the maximum ADC data around 600 to 800 codes.
Best regards,
Cash Hao
had tried for an good adc capture ..where i have changed my capaure duration to 32us and reduced gain to 2.6db where i repeately got the error as
| DToF - Shift value was greater than maxSampleShift |
...how ro solve this error






HI,
You can change this parameter USS_ALG_MAX_SAMPLE_SHIFT in the code to avoid this error. By default it should be 20, you can try with 40/60/80.
Best regards,
Cash Hao
Hello forum,
now i got my graph in below...i didnt change any parameter even in above mention uss_alg_max_sample_shift .....because i didnt get any error while run with same paremter in today start of my work




anything i still need to change ....
**Attention** This is a public forum