This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I have a problem with my FET it lights red even when it's disconected from my MSP430FR6047, does anyone experienced something similar before, and how do you fix it.
Thank for you help.
Is its programming function affected?
Normally CCS will automatically update its firmware.
Yes, but we think the problem is internal on the JTAG, because either it's conected or not the red led is on
If this is a hardware fault, then I have no idea.
But you can try to update the firmware manually first. The following is a lite tool you can use.
I'm not sure if this is the solution, I mean I did it and the FET is working now, but that also happens when I restart my pc
Is there a fixed way to definitely reproduce it? If you can fix it via updating firmware, then you may need to check the environment(software, driver...)
So you cannot resolve the problem via updating firmware? And when you use another FET it works well?
Then I think it should be a hardware issue.
**Attention** This is a public forum