This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-FET: MSP-fet is not recognize as a com port but as HID ; VID 2047 and PID 0204

Part Number: MSP-FET

Good morning, 

I looked in the forum but could get an answer. 

I ordered 3 new MSP FET (the black ones) and connected them. They are recognize as a com port, everything is fine. 

I tried to use them thru MSP430 flasher; They rebooted and now, they do not show as a com port but as an HID with VID 2047 and PID 0204.

Same issue with all 3 new programmers. 

Please help. 

Thank you

  • Hello, 

    I fixed my problem. 

    If this happen to you, please do the following : 

    install mspFlasher (if not already) and try to erase something using : MSP430Flasher.exe -eEraseAll

    You do not need to connect anything on the programmer. This command will try to communicate with the MSP FET, find there is a corrupted firmware, fix it and update it ! 

    And voila ! 

    Hopefully this will save some time to someone ! 

    Have a good day

  • Hi Benoit,

    Great! Glad you were able to resolve your issue.

    Thanks!

    -Mitch

**Attention** This is a public forum