This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F2618: MSP-FET driver chances automatically from COM/LPT section to HID section

Part Number: MSP430F2618
Other Parts Discussed in Thread: MSP-FET

Tool/software: Code Composer Studio

Hi,

I have 2 new MSP-FET debug devices. For that reason I installed CCS 9.0.1.00004.

After connection of the first MSP-FET, the drivers was shown in the right section of the device driver window: LPT & COM.

After starting CCS and try to start the debugger, the driver disapears from LPT & COM and new drivers apears in Human Interface devices.

The debugger does not start.

Same with the second MSP-FET device.

Any suggestions?

Thx, Manfred

  • Hi Manfred,

    Make sure the MSP-FET is plugged into a USB 2.0 port directly into your computer (not a USB 3 port or USB hub)

    Are you using a custom board to connect the MSP-FET to? If not, what TI EVM are you using?

    Thanks,

    -Chris

  • Hi Chris,

    thank you for your answer.

    I tried also with USB2.0 and it was the same.

    Until last week I worked with IAR 5.40 workbench and the older MSP-FET430UIF (grey one).

    Because of hardware defect I ordered the successor type MSP-FET (black one) because of thwe old one is not available anymore.

    But the new one is not compatible to IAR 5.40. For that reason I installed the CCS 9.

    As I described, first plug in of the MSP-FET install the right drivers and it is shown in the device manager under COM & LPT with reasonable driver names "MSP....".

    After try to start the debug session with CCS, the drivers in COM/LPT desapears and immediately 2 new drivers apears in the HID area.

    After that it is not possible to change the driver back to the original driver because Windows tells me the driver is not a HID driver.

    If I uninstall the device and connect it again, the HID driver is installed again :-(

    I have connected the MSP-FET to my hardware, which was used also with the old debug device.

    Any idea, whow I can remove the HID driivers und install the original again?

    Regards,

    Manfred

  • Hi Manfred,

    Have you attempted checking in the Windows device manager under Human Interface Devices to install the HID drivers?

    -Chris

  • Hi Manfred,

    Were you able to resolve your issue?

    -Chris

  • Hi Chris,

    yes, thank you.

    I installed the MSP430Flasher on another PC and there it was possible to flash the firmware into the MSP-FET.

    Now both devices are working also on my PC.

    Manfred

**Attention** This is a public forum