Other Parts Discussed in Thread: ADS1178, MSP430F5131
Dear All,
Iam in need of a general purpose microcontroller with the following features. I thought MSP430 will have such a configuration but i didn't find any. Some of them are having ADC DAC etc.. I don't have any problem in having an ADC, the cost is the only constraint. The cost of the controller should be less than 0.5~0.6 USD for the following features
1. Programmable clock output of 20 MHz - 1 No . For this iam even planning to use the clock from an SPI interface ( if MSP is not having a programmable clkout Pin)
2. UART
3. GPIO - 25 Pins
4. External Interrupts - 3 or 4
I found a 8051 microcontroller STC11F02 by www.stcmcu.com, which satisfies my requirement but the fact is that i would like to choose a TI product
due to its reliability.
http://www.mcu-memory.com/datasheet/stc/STC-AD-PDF/STC11F-10Fxx.pdf
Please suggest an MSP430x
Thanks a lot
Shasthri