Part Number: MSP430F5359
Hello,
Our embedded team encountered an issue with not appropriate RESET on our systems.
When performing FW update for our devices in field 3-4% of the devices are stacked and stopping to work.
Same Hardware, same Firmware - The system not providing correct RESET and enters to interesting mode:
- On several input/output pins we observed strange pulses or waveforms @ frequency of 4.8309 Hz (207 msec).
- The processor is not responding on RST/NMI pin.
- Only Power Cycle can end this condition.
We have not any code in BSL or application providing this kind activity on I/O.
What is can be?
Any clue?
Thank you in advance,
Best Regards
Radislav Yanai