Part Number: MSP430F147
Tool/software:
The issue is using an updated compiler when programming old source code to our MSP430F147. The original hex file works with the FET programming application, but loading the file using Code Composer Studio doesn't work. It loads perfectly to the micro, but the memory seems affected because the default settings aren't what they're supposed to be. I can't tell which memory locations are shifted between the original since I cannot run the original compiler and use the debugger. What are the significant differences between compiler TI v4.2.7 and TI v3.2.2.1.8?
Any help would be greatly appreciated.