This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Detail of my output.txe.txt :
* -----/|-------------------------------------------------------------------- * * / |__ * * /_ / MSP Flasher v1.3.11 * * | / * * -----|/-------------------------------------------------------------------- * * * Evaluating triggers...done * Checking for available FET debuggers: * Found USB FET @ COM9 <- Selected * Initializing interface @ COM9...done * Checking firmware compatibility: * FET firmware is up to date. * Reading FW version...done * Setting VCC to 3000 mV...done * Accessing device...done * Reading device information...done * Loading file into device... # Exit: 59 # ERROR: File end error * Starting target code execution...done * Disconnecting from device...done * * ---------------------------------------------------------------------------- * Driver : closed (No error) * ---------------------------------------------------------------------------- */
my hex size is 87.3 KB.But hex translate TI txt ,this is fine .How can I solve this problem?
Hi,Ryan
Attachment is my hexfile and my target IC is MSP430F147. I use MSP-FETFLASH Emulation Tool to connect MSP430F147 and my Msp430-Flasher version is 1.3.11. If you can load hex,please tell me.hexfile.7z
Thank you!
**Attention** This is a public forum